LTE FDD
This topic describes carrier settings for Real-Time capability.
All carrier settings are read-only when the real-time carrier state is on because only one real-time carrier is available for this release (A.14.00).
Wherever <carrier> appears in the SCPI command descriptions of this topic, that value is fixed to 1 for this release (A.14.00).
<carrier> is constructed from Carrier ID and Carrier Type.
Displays the enable state of a carrier.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>[:STATe]? |
|
SCPI Example |
RADio:LTEF:WAVeform:RTIM:CCAR? |
|
Notes |
Query only |
|
State Saved |
Yes |
|
Preset |
ON |
|
Initial S/W Revision |
A.14.00 |
This setting returns the carrier type. This setting is automatically set when a carrier is added.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:TYPE? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:TYPE? |
|
Notes |
SCPI only, Query only Returns FDDULEUTRA |
|
State Saved |
No |
|
Preset |
FDDULEUTRA |
|
Range |
Uplink E-UTRA |
|
Initial S/W Revision |
A.14.00 |